Technical FAQs

Ask a Question

Osisense XC special - Cross-reference of the obsolete XF9FC2, XF9GC2 and XF9HC2 overtravel power switches

The obsolete XF9FC2 (Ith = 80A), XF9GC2 (Ith = 125A) and XF9HC2 (Ith = 200A) overtravel power switches, in automatic resetting, are replaced by the XF9F1152 switch (Ith = 200A). Attached corresponding data sheet. The metal box of the new power switch has bigger dimensions than the obsolete enclosure. Arms have the same lenght.

Was this helpful?
What can we do to improve the information ?