Technical FAQs

Ask a Question

Osisense XC special - Cross-reference of the obsolete XF9FC1, XF9GC1 and XF9HC1 overtravel power switches

The obsolete XF9FC1 (Ith = 80A), XF9GC1 (Ith = 125A) and XF9HC1 (Ith = 200A) overtravel power switches, with manual resetting, are replaced by the XF9F1151 switch (Ith = 200A). Attached corresponding data sheet. The metal box of the new power switch has bigger dimensions than the obsolete enclosure. Arms of the new switch is longer than the old one.

Was this helpful?
What can we do to improve the information ?