Browse FAQs

Preventa XCS - Data sheet of the XCSM3902L10 red limit switch

Published date: 24 September 2019

The XCSM3902L10 red limit switch reference is not shown into the catalogue. It is in fact a XCSM3902L* with 10m cable lenght. Attached the available data sheet of the XCSM3902L5 limit switch coming with 5m cable lenght. If you need the CAD file of the XCSM3902L10 part number, please use the existing CAD of the standard XCSM3902L1 or XCSM3902L2.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.