Technical FAQs

Ask a Question

Does Schneider Electric offer a PLC module with IPsec capabilities?

Title
M580 and IPsec capability
 
Issue
M580 and IPsec capability
 
Product Line
M580 BMENOC03x1
 
Environment
Unity Pro 11 or higher
 
Cause
N/A
 
Resolution
 Yes, Schneider does have a M580 PAC Communication module, BMENOC0301, that has IPsec capabilities.
Attached is the M580 BMENOC03x1 user manual. Please reference the Configuring IP Secure Communications information under Section 4.4 Security.



 
Was this helpful?
What can we do to improve the information ?