Technical FAQs

Ask a Question

Does the M340 or M580 PLC have a Profinet module?

Title
M340 or M580 PLC and Profinet
 
Issue
M340 or M580 PLC and Profinet
 
Product Line
M340 M580
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 No, The M340 or the M580 do not have a Profinet module. The only supported protocol is Profibus DP and requires to use of the Profibus Remote Master Gateway (TCSEGPA23F14F)
Was this helpful?
What can we do to improve the information ?