Technical FAQs

Ask a Question

Does the M340 or M580 PLC have a Profinet module?

Title
M340 or M580 PLC and Profinet
 
Issue
M340 or M580 PLC and Profinet
 
Product Line
M340 M580
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The M340 and the M580 do not have any Profinet or Profibus capable in-rackmodules. The only supported protocol is Profibus DP and requires to use of the Profibus Remote Master Gateway (TCSEGPA23F14F)
Was this helpful?
What can we do to improve the information ?