Technical FAQs

Ask a Question

Osisense XC - Data sheet of the adapted switch XCKN2118G11S37

XCKN2118G11S37 adapted switch is based on the standard XCKN2118G11 limit switch. The rotary head is turned 90° and the roller lever is reverted like shown in the attached picture. He has the same characteristics as the standard XCKN2118G11 switch. It comes with a plastic cable gland Pg11. Attached the XCKN2118G11 data sheet.

Was this helpful?
What can we do to improve the information ?