Technical FAQs

Ask a Question

Issue with Profibus Remote Master Gateway DTM and M580 using Unity 11

Title
Profibus Remote Master Gateway DTM and M580 using Unity 11
 
Issue
Profibus Remote Master Gateway DTM and M580 using Unity 11
 
Product Line
M580 and PRM Gateway
 
Environment
Unity Pro 11 or higher
 
Cause
N/A
 
Resolution
When you open Unity it states that the DTM catalog has to be updated and then Unity hangs and stops on update of Se_GatewayPrmDtm.DtmCore.1 .
That is a known issue with PRM version 1.2.12.0; this was resolved with PRM Profibus Remote Master Gateway DTM version 1.2.13.0

 
Was this helpful?
What can we do to improve the information ?