Technical FAQs

Ask a Question

Osisense XC - Data sheet of the adapted switch XCKN2118P20SER

XCKN2118P20SER adapted switch is based on the standard XCKN2118P20. The rotary head is turned 90° and the roller lever is reverted like shown in the attached picture. He has the same characteristics as the standard XCKN2118P20 switch. Attached corresponding data sheet.

Was this helpful?
What can we do to improve the information ?