Technical FAQs

Ask a Question

What is the recommended replacement for the Magelis MPCEN05NAX00N, control module, and MPCNT50NNN20N, panel display?

Issue:
What is the recommended replacement for the Magelis MPCEN05NAX00N, control module, with MPCNT50NNN20N, panel display?

Product Line:


Environment:


Cause:


Resolution:
Our suggested replacement would be: 
HMIBMPHI74D4801 + Power supply HMIYMMAC1 + HMIDM7421 display.

Keep in mind that the cut-out dimension of the replacements are not the same as the original.
Was this helpful?
What can we do to improve the information ?