Technical FAQs

Ask a Question

Preventa XU - What is the sensing distance of the XUSZLPE laser alignment ?

Please note that such data is not provided into the catalogue, because the sensing distance of the XUSZLPE laser alignment is 100 meters, higher than the XUSL4E-2E maximum nominal range of detection. Such value is indicated into the XUSL4E-2E user manual, at the end of the document. Attached user manual extract.

Such device is powered by 2 batteries 1.5V LR03 type or AAA format. If the performance of sensing distance is reduced strongly, please replace them by new ones.

Was this helpful?
What can we do to improve the information ?