Technical FAQs

Ask a Question

What is the replacement for the Quantum 140CPS11410 power supply?

The replacement is the Quantum 140CPS11420 power supply. Both power supplies are 115/230 Vac.
The Quantum 140CPS11410 has a current rating of 8A.
The Quantum 140CPS11420 has a current rating of 11A.
Was this helpful?
What can we do to improve the information ?