Technical FAQs

Ask a Question

Does the 140CRP31200 module get counted with regards to maximum number of allowable Quantum communication cards in a Unity project?

Title
Quantum 140CRP31200 module
 
Issue
3Unity Pro
 
Cause
N/A
 
Resolution
 No, The 140CRP31200 module does not count towards the total maximum number of Quantum communication cards in a Unity project.
Was this helpful?
What can we do to improve the information ?