Technical FAQs

Ask a Question

Video: How to connect to a MiCOM Px40 relay using ethernet or the front panel DB-9 port

Issue
The user would like to connect to a Micom Px40 relay to view settings files, disturbance records, event logs and supervise the relay remotely.
 
Product line
MiCOM Px40
 
Environment
Easergy Studio V6.0
 
Resolution
The video below explains how to connect to a MiCOM Px40 relay using Ethernet or the serial front panel DB-9 port. The video assumes that the relay's Ethernet connection had been configured correctly. 

Was this helpful?
What can we do to improve the information ?