Browse FAQs

What can caused an "Application has halted In java class gp classes.graphics.cp" error on a Magelis HMIG5U?

Published date: 31 July 2019

Issue
"Application has halted In java class gp classes.graphics.cp"

Product Line
Magelis HMIG5U

Resolution
A corrupted runtime can cause this error.
The solution is to unlock the HMIG5U and re-install the Vijeo Designer Runtime.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.