Technical FAQs

Ask a Question

What causes ProWORX 32 printing error "Physical Database Not Found"?

Printing a ProWORX 32 project could result in the error "Physical Database Not Found". The reason for this is because something (i.e., spyware protection, anti-virus protection or a firewall) on the PC prevented two Crystal Reports files from getting installed.

`P2smon.dll` version 8.6.1.179
`p2bdao.dll` version 8.5.0.7

This problem has been corrected in ProWORX 32 v2.1 Patch B. The patch re-installs the files.
Was this helpful?
What can we do to improve the information ?