Browse FAQs

Can I make a change to the traffic cop in a Quantum PLC while the PLC is running using Proworx Nxt, Proworx 32 or Concept?

Published date: 30 January 2019

Issue
Traffic Cop change to Quantum while running

Product Line
Modicon Quantum 

Enviroment
ProWORX NxT, ProWORX 32, and Concept

Resolution
No, you must stop the Quantum PLC to make a change to the traffic cop using Proworx Nxt, Proworx 32 or Concept.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.