Technical FAQs

Ask a Question

What Quantum modules support NTP ?

Title
Quantum modules that support NTP
 
Issue
Quantum modules that support NTP
 
Product Line
Quantum
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
The NTP service is not available on the Quantum CPU Ethernet port.
You will need to use a 140NOE77111 module or a 140NOC78000 module that supports the NTP service.
Also the 140CRP31200 QEIO Remote Processor module does support NTP but will require the use of a QEIO capable Connexium managed switch to connect your external NTP Server to a DIO port.
Was this helpful?
What can we do to improve the information ?