Technical FAQs

Ask a Question

What is the difference between BMXNOC0401 vs BMXNOC0401.2 ?

Title
Difference between BMXNOC0401 vs BMXNOC0401.2
 
Issue
Difference between BMXNOC0401 vs BMXNOC0401.2
 
Product Line
M340 BMXNOC0401.
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
The difference between a BMXNOC0401 and a BMXNOC0401.2 is the firmware version on the module.
The .2 extension indicates that the firmware is 2.0 or greater. The part number BMXNOC0401 is for original 1.0 firmware modules.
Today, all modules are manufactured with a firmware greater than 2.0, therefore you would select the BMXNOC0401.2 device.
Was this helpful?
What can we do to improve the information ?