Browse FAQs

Vijeo Designer Snap to Grid needs to be disabled twice before it is actually disabled

Published date: 22 May 2019

Issue:
Vijeo Designer Snap to Grid needs to be disabled twice before it is actually disabled

Product Line:
Vijeo Designer (all versions)

Resolution:
When you need to draw something free hand and need to disable the "Snap To Grid" feature, you will need to Disable the feature twice. That is, you need to disable it, re-enable it, and then disable it again. This is a known bug in Vijeo Designer that has not been resovled.



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.