Technical FAQs

Ask a Question

HHF files must have a period between 1 and 60 minutes and evenly divisible into 60

Issue
The user is exporting revenue data using ION Setup into .hhf file format.  However, they get the following error message:

          
          HHF files must have a period between 1 and 60 minutes and evenly divisible into 60.

Product Line
ION Meters

Environment
ION Setup

Cause
The software reads the last two records and takes the difference between the two.

Resolution
This problem will happen when there is not yet two records in the meter.  Check Load Profile (Revenue Log) to make sure there is enough records in the data recorder.
 
Was this helpful?
What can we do to improve the information ?