Technical FAQs

Ask a Question

Does the Generic Windows PC Vijeo Designer Runtime Target support Datalogging?

Issue:
Does the Generic Windows PC Vijeo Designer Runtime Target support Datalogging?

Product Line:
Vijeo Designer (all versions)

Resolution:
Yes, the Generic Windows PC target in Vijeo Designer does support Datalogging. It is essentially the same platform as a Magelis iPC series which also supports the functionality available.
Was this helpful?
What can we do to improve the information ?