Technical FAQs

Ask a Question

What is the maximum number of words that can be use with Advantys via Peer Cop?

The length of Peer Cop’s global output/specific input varies depending on the actual configuration of I/O words in the island. The lengths will be limited to 32 words at maximum—any additional words will be cut off.
Was this helpful?
What can we do to improve the information ?