Technical FAQs

Ask a Question

Video: How do I enable Symbols in ProWORX 32?

Below are the steps required to enable Symbols in ProWORX 32:

1- Open the project properties. From the main toolbar, go to PROJECT then PROPERTIES.
2- Select the PROJECT tab.
3- Check off the box for ENABLE SYMBOLS.
4- Click the APPLY button, then click on the OK button.

The Symbols will now show up in the Logic screen and the Documentation window.

Was this helpful?
What can we do to improve the information ?