Technical FAQs

Ask a Question

What is the pin assignment wiring for VW3A8306TF10 adapter ?

The pins that are wired are pin 4, pin 5 and pin 8.

See attached file for drawing.


rev 2-20-18
Was this helpful?
What can we do to improve the information ?