Technical FAQs

Ask a Question

How is Service Pack 2 applied to Proworx 32 v2.1?

Issue:
  Updating Proworx 32 2.1 to SP2

Resolution:
  Launch the Service Pack executable and choose the <Repair> function to apply SP2 to Proworx 32 v2.1
Was this helpful?
What can we do to improve the information ?