Technical FAQs

Ask a Question

Open Phase Detection Framework: Detailed Explanation

Issue
To detect meter installation faults.

Product Line
ION8650

Environment
Designer, Meter Template

Cause
One or two voltage inputs are floating on a blade powered meter.

Resolution
Refer to the attached PDF for detailed explanation on the framework including calculations.  The document was published on July 2015.
 
Was this helpful?
What can we do to improve the information ?