Technical FAQs

Ask a Question

Extra Modules Group in Designer for ION8650 Meter with Firmware v004.020.001

When viewing the template of an ION8650 (A/B/C) meter with firmware v004.020.001 in Designer, an 'Extra Modules' group gets created with certain modules that belong to specific frameworks.

Product Line
ION8650 v004.020.001 (any option)

Designer (PME8.0, PME8.1)

Incorrect node diagram

*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

The attached zip file contains the correct node diagrams.

1. Download and unzip the attachment.  It contains the following folders, each with a .CFG file.


2. Copy the node diagrams to their corresponding folder under ...\System\Diagrams\nd.

NOTE: Make a copy of the existing node diagrams to have the original files to revert back.

3. Delete the node diagram for the meter in ...\Config\Diagrams\nd folder.

Now the modules will appear in the proper groups.

Was this helpful?
What can we do to improve the information ?