Technical FAQs

Ask a Question

When using redundant 140CPS12400 power supply's, can I safely remove one of them from the backplane without disturbing the process?

Issue: N/A
Product Line: Quantum
Environment: N/A
Cause: N/A

Answer: Yes, you can safely remove one of the two 140CPS12400 supplies without impacting the process.. This is also true of the 140CPS12420 power supplies.

Was this helpful?
What can we do to improve the information ?