Technical FAQs

Ask a Question

Does Schneider Electric offer the Brushless DC drives type BLP14, BLV14 or brushless dc motors such as RECM or BDM?

The Brushless DC motors and drives that are offered by Schneider Electric in Europe are not available here in North America
Customers looking for spare BLP14 brushless dc drives should contact the OEM machine builder for spares.
Also customers looking for spare brushless DC motors including RECM, or BDM motors should also contact the OEM machine builder due to the fact that these are also only offered in Europe.

 
Was this helpful?
What can we do to improve the information ?