Technical FAQs

Ask a Question

What is the maximum number of devices supported by the 140NOC78000 module?

Title
Maximum number of devices supported by the 140NOC78000
 
Issue
Maximum number of devices supported by the 140NOC78000
 
Product Line
Quantum 140NOC78x00
 
Environment
Unity Pro

Cause
N/A
 
Resolution
 The maximum number of devices that the 140NOC78000 module can support through the Unity DTM Browser is 128 devices (125 devices as scanner + 3 devices as adapter) This number of devices is shared with Modbus TCP capable devices. See attached document for complete details
Was this helpful?
What can we do to improve the information ?