Technical FAQs

Ask a Question

Is it possible use M580 HSBY in architecture with no RIO?

Yes, it is an acceptable architecture for M580 HSBY. Refer to the attached architecture as an example from the M580 HSBY manual.
In this regard, M580 HSBY is different, compare to Quantum HSBY (which RIO link is required).
Was this helpful?
What can we do to improve the information ?