Browse FAQs

How to download and install Somove V2.x on a PC?

Published date: 14 August 2019

Evolve from SoMove Lite 1.x to SoMove 2.x assures more flexibility for updates
 
This FAQ gives detailed explanations for :
> Installation of SoMove V2.0,
 
 
 
How to install SoMove V2.0
In order to configure or connect to a device, the corresponding DTM library MUST be downloaded and installed on the computer, as well as SoMove FDT.
SoMove V2.0 software and DTM libraries are available on the below link:
 
https://www.schneider-electric.com/products/ww/en/5100-software/5105-configuration-software/2714-somove/
 
Follow the steps in the attached manual or download the SoMove V2.xx installation notes.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.