Technical FAQs

Ask a Question

How come the export option is not available or grayed out in Vijeo Designer to the project to VDZ?

Issue:
How come the export option is not available or grayed out in Vijeo Designer to the project to VDZ?

Product Line:
backup, export, application, project, Vijeo Designer

Environment:


Cause:


Resolution:
 The export feature will not be available when the project is open.   The project needs to be closed when using the export feature.
Was this helpful?
What can we do to improve the information ?