Technical FAQs

Ask a Question

Do Unity Momemtum PLC double word datatypes have to be located on an even starting address?

Yes, double word registers such as REAL, DWORD, DINT and UDINT must be located on an even 
starting address when using the Unity Momemtum PLCs.
Was this helpful?
What can we do to improve the information ?