Browse FAQs

Can't modify / edit the name of the Device DDT attached to a module added in CCOTF while using Unity Pro

Published date: 15 February 2019

Issue
After adding a module using CCOTF the device name can not be modified.

Product line
Unity Pro, Control Expert, M580, Quantum

Resolution
Unity Pro as recent as 13.1 did not include this functionality. The ability to modify the Device DDT variable name using CCOTF will be added with the initial release of Control Expert which is version 14 (technically Unity Pro v14).


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.