Technical FAQs

Ask a Question

PME 8.0 - Full Dial appears with text overlapping the dial when viewed from Web Application

Issue
When a Full Dial object is viewed in Web Applications it appears with the dial's text on top of the dial and out of alignment as shown in the image below. There are no rendering issues when viewed in Vista.


Product Line
Power Monitoring Expert 8.0

Environment
Web Application

Cause
This is a known issue with partial dials in PME 8.0

Resolution
There is no workaround at this time for PME 8.0, however the issue has been resolved in PME 8.1. 
Was this helpful?
What can we do to improve the information ?