Technical FAQs

Ask a Question

Is the point count for each type binary and analog (BI, AI, etc...) limited to 2048 points as specified in DNP driver help in Vijeo Citect 7.xx and 2015?

You may have address tags above 2048 poins.The DNP driver documentation is not correct and disregard the index limit.
Was this helpful?
What can we do to improve the information ?