Technical FAQs

Ask a Question

Where is the link to download latest intermediate firmware exec for converting CPU from unity to concept (140CPU43412U to 140CPU43412A) ?

Intermediate exec to upgrade CPU from Unity to Concept is attached.
use Unity_to_Concept_43212A.bin  if the CPU module is up to PV15.
use Unity_to_Concept_43212PVGE16.bin if the CPU module is PV 16 or higher.

Use the Unity Loader to load the intermediate EXEC.
Use the Concept EXECLoader to load the Q5rv144E.bin.
Was this helpful?
What can we do to improve the information ?