Browse FAQs

What is the replacement for a drive side connector AEOCON009 used with the Lexium 17 drives?

Published date: 04 December 2018

Issue: Replacement


Product Line: Lexium BPH


Environment:


Cause: Obsolescence


Resolution:

What is the replacement for a drive side connector AEOCON009 used with the Lexium 17 drives?

The connector bearing part number AEOCON009 used with the Lexium 17 drives is obsolete.

The drive side connector is a Phoenix connector and the vendor part numbers are listed below.

Back Shell : KGS-PC4/6-F
Connector : PC-4/6-ST-7.62
 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.