Browse FAQs

What is the Ethernet TCPIP card for the Altivar Process drive?

Published date: 01 March 2019

Issue:
Wants to add Ethernet TCPIP communications to the ATV Process Drive

Product line:
Altivar Process, ATV630, ATV650

Environment:
All

Cause:
Catalog selection

Resolution:
The part number is VW3A3720, Ethernet/IP, ModbusTCP communication module - 2RJ45

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.