Browse FAQs

How to configure your TeSys T using SoMove

Published date: 30 November 2018

The purpose of the FAQ is to show you where are located the different setting parameters when using SoMove configuration tool.
If you have additional question you can use also “TeSys T help” embedded in SoMove help.
 
You must always have the latest SoMove version screen copy done in November 2015
 
Note that the configuration tool (generic name "SoMove") is based on the FDT/DTM architecture, thus is in fact composed of two components
- The FDT container : SoMove
- The DTM Device Type Manager : there is one single DTM for both the TeSys U and the TeSys T 

Most recent versions of each of these components shall be installed on your laptop.
See attachment for example

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.