Browse FAQs

Is there a protective module for the M340 rack?

Published date: 16 August 2019

 The Modicon M340 PLCs have an IP20 protection degree and they have been tested with pins. It is an enclosed equipment. It may, therefore, be installed withoutcasing in restricted access rooms not exceeding pollution level 2 (control room with neither machine nor activity producing dust).

NOTE: for a rack to be compliant with the IP20 protection degree, the empty module slots must be protected by a BMX XEM 010 protective cover. See product specification for the BMX XEM 010 below.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.