Technical FAQs

Ask a Question

Can I move Unity Pro Project Settings from one project to another?

Yes, you can export the Project Settings to an .XSO file and import them into another project.
<Tools><Project Settings> <Export>.

This can be done with the Options as well exporting them to an .XOO file to be imported into another Unity Pro session.
<Tools><Options> <Export> at the bottom of the page.
Was this helpful?
What can we do to improve the information ?