Browse FAQs

Which Modbus TCP Function Code are support by the M340 as a Server (Slave)?

Published date: 16 August 2019

The M340 accepts FC 1,2,3,4,5,6,15,16,23 when configured as Modbus TCP Server (Slave).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.