Browse FAQs

Are the Quantum IO status table words configurable in Unity Pro?

Published date: 05 July 2019

The start of the status table is configurable for each drop in Unity Pro.

However, the length is not configurable.
Unity Pro assumes a worst case scenario of a Quantum drop using two 16-slot racks which would
require 16 words, one byte per slot.  
The starting address plus the next fifteen registers is automatically designated.
This is fixed and cannot be changed.
________________________________________________

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.