Technical FAQs

Ask a Question

Is there a way to run the Unity v10 simulator on a Windows XP sp3 platform?

One of our customers discovered the following when running Unity Pro v10 on a Windows XP sp3
operating system which is not a qualified platform for Unity Pro v10.

Before launching the simulator by connecting within Unity Pro
Start / All Programs / Schneider Electric / SoCollaborative / Unity Pro / PLC Simulator,

Run C:\Program Files\Schneider Electric\Unity Pro\PLC_Simulator\debugger.exe.

The simulator should behave normally.

Was this helpful?
What can we do to improve the information ?