Is there a document that explains the issues with IO Scanner and the TSXETG100, EGX100SD or ModbusTCP to Serial gateway?
Title
IO Scanner and the TSXETG100 or EGX100SD
Issue
IO Scanner and the TSXETG100 or EGX100SD
Product Line
M580, M340, Quantum, Momentum
Environment
Unity Pro
Cause
N/A
Resolution
Attached is a document that explains the issue with using the IO Scanner service of the NOE modules to comunicate through a TSXETG100, EGX100SD or a Modbus TCP to Modbus serial gateway.
Sign up for all the latest solutions, offers and best practices straight to your inbox.
All done!
Thank you for subscribing to updates from Schneider Electric.
We are excited that you have joined the group. You will receive your welcome email soon describing the program and what to expect in the upcoming weeks. Enjoy!