Updating an M580 CPU version 1.1 to CPU v2.0. Unity Pro versions 8.0, 8.1 or 10.
Issue:
An M580 application with CPU v1.1 developed with Unity Pro v8.0, 8.1 or 10.0 cannot be udated to CPU v2.0 due to compatibility
issues. The 'Change CPU' option is not permitted.
Resolution:
The solution is to export/import variables and program code into a new application.