Technical FAQs

Ask a Question

What does Unity Pro 'expression expected' error mean?

Issue:
  This error ususally occurs on a Build when a pin on a function block is not configured.

Resolution:
  Double click on the error in the output window and it will take you to the code that needs to be corrected.
Was this helpful?
What can we do to improve the information ?